5/11/2018 2:22 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Thank you Pete; You seem to have understood quite correctly the access of FM 353 parameters: you cannot use the on-board connector through an adapter to configure the FM 353. This is done with FM 353 parameterization software, through the CPU onnection. Look at the attachment, from the FM 353 manual. It shows that the on-board connector of the FM 353 is used to connect to the drive you want to control, and the parameters are loaded from a software package to the CPU. https://support.industry.siemens.com/cs/ww/en/view/60677209 Here is a link to the last version of parameterization siftware for the FM 353 and FM 354; it works with Win 7 64-bits: Configuration Package FM 353 and FM 354 Version 4.03.09 Software/Hardware Prerequisites
and one of the following operating systems:
https://support.industry.siemens.com/cs/ww/en/view/60605765 Hope this helps, Daniel Chartier |
5/11/2018 11:21 PM | |
Posts: 14 Rating:
|
here are some links to help give you some more background around the issue I think I am having: https://support.industry.siemens.com/cs/ww/en/view/4333938 This link is what siemens sent me : https://support.industry.siemens.com/cs/ww/en/view/299182 So I purchased the PC Adapter V5.1 with MLFB 6ES7972-0CA23-0XA0 as it suggests. Problem is it has a red light on it and is also not compatible with WIN 7 and as such I cant get a connection to cpu at all. ( I guess that's because this link is so old. So im just trying to figure out which adapter I should get now |
Last edited by: Jen_Moderator at: 5/14/2018 8:18:43 AMOptimized links. |
|
5/12/2018 10:10 AM | |
Posts: 14 Rating:
|
Hey guys, I still need help with this issue as I'm unsure which adapter will. Do the job.. If anyone knows how to figure that out please let me know! |
Follow us on