4/15/2016 6:56 AM | |
Joined: 10/2/2013 Last visit: 8/25/2025 Posts: 339 Rating:
|
try for first put that %IWXXX:P to some WORD area, f.ex.%MW40, after that watch that %MW40. There you can see it's value. please refer below topic this may help you,
|
Technology is best when it brings people together,so we are here now :) |
|
This contribution was helpful to
1 thankful Users |
4/15/2016 7:31 AM | |
Joined: 11/26/2015 Last visit: 2/19/2025 Posts: 92 Rating:
|
Hi, Ankurgamit, Actually I have tried using mov function to move the AI input value from IW6 to a memory address MW100, and I also monitor IW6:P and MW100:P in the watch table, but the values are all 128. I was quite confuse about this, if the value can be monitored, then it should be changed, if cannot, why there was a value of 128? Thanks.
|
Follow us on