4/8/2016 1:55 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Why would you like to switch off and on power several times? You can simply program a button to exit runtime or to disconnect the connection to PLC. The best practice is to keep the power source stable as much as you can, so it is recommended no only to keep it on but also to power it from DO UPS. please see note in the footer of page 4 for this document. https://www.automation.siemens.com/salesmaterial-as/brochure/en/brochure_panels_en.pdf |
Ayman Elotaify |
|
4/8/2016 3:28 PM | |
Posts: 8946 Rating:
|
With panels and Windows-CE Panels i never have had problems due switching off the Panel. It is different from Winows - RT PC's. |
4/24/2016 12:45 PM | |
Posts: 487 Rating:
|
Hi In my opinion the biggest problem is switching a the device of during start-up and of cause power dips and spikes Eric |