8/7/2013 8:29 PM | |
Posts: 47 Rating:
|
After hours and hours of trial and error I finally found at least a partial solution. What I did: LOGO! PLC connected to my router at fixed IP address 192.168.1.90 (IP setting in LOGO!) Local PC connected to my router at fixed IP address 192.168.1.99 Forward port 10001 to my local PC in stead of the LOGO! in the router Forward IP address 192.168.1.99 port 10001 to IP address 192.168.1.90 port 10001 For the latter I used a linux utility called rinetd, which is also available for windows, seehttp://mattiasgeniar.be/2010/04/14/tcp-traffic-redirection-on-windows/ So now the data traffic goes through my router, then through my PC and then to the LOGO! This works. I wonder however why it does work this way and not directly from router to LOGO! Maybe someone has a clue about that? Thanks, Dion
|
This contribution was helpful to
1 thankful Users |
6/28/2015 11:58 AM | |
Joined: 11/14/2012 Last visit: 10/28/2024 Posts: 8 Rating:
|
Hi very thanks for your description. my problem is solved by you. |
This contribution was helpful to
1 thankful Users |
7/1/2015 5:27 PM | |
Posts: 45 Rating:
|
thank you for details but I get the external IP address of my router and I can not log in to my router outside let alone my logo what should we do? |
11/2/2015 3:10 PM | |
Joined: 8/21/2014 Last visit: 9/12/2025 Posts: 1087 Rating:
|
New question published by Dana 1987 is split to a separate thread with the subject Establishing a connection between LOGO and Smartphone by WiFi?. Best regards |
My Forum is the place to personalize your profile, |
|
12/8/2015 10:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by Herman (NCP) is split to a separate thread with the subject Access 4 Logos from the Interent. Best regards |
Follow us on