9/9/2022 7:47 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4108 Rating:
|
Hi Programmer_Lte, the state "Partly running" shown in SIMATIC Runtime Manager is not related to a missing license. This means your project has caused some errors which prevents the runtime form starting. Mostly this is caused by some compiling issues. To ensure a complete re-compile, delete the folder 'IM\HMI' inside your TIA Portal Project using Windows Explorer. But as far I know, you would need S7-PLCSIM Advanced to connect the WinCC Unified simulation to a simulated PLC. See FAQ 109793854. Kind regards |
This contribution was helpful to
1 thankful Users |
9/12/2022 9:14 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4108 Rating:
|
Hi Programmer_Lte, do you still have the state "Partly running" shown in SIMATIC Runtime Manager? If this is your first WinCC Unified project you are testing, then please try to simulate a new project with nothing more than a blank screen. This is to ensure your system is able to run a simulation. When this is working, or it's not your first project, please use the RTIL Trace Viewer and filter for severity "Fatal" and "Error". Maybe you will find the cause for the "Partly running" in this way. If not, I suggest creating a new support request. Meanwhile, I have tested the simulation using S7-PLCSIM instead of S7-PLCSIM Advanced and yes, this is possible with V17. To get the HMI connection running, the settings for the PG/PC Interface has to be set to S7ONLINE (STEP 7) --> PLCSIM.TCPIP.1. Kind regards |
Last edited by: Stefan Arcularius at: 09/12/2022 09:21:17Added link to system manual |
|
9/12/2022 2:00 PM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4108 Rating:
|
Hi Programmer_Lte, I'm concerned about the "Partly running" state. I'm quite sure this is not related to the used communication. I believe the runtime has not yet started communication when the error occurs. Maybe you have some troubles with your installation. Have you already installed update 4 for TIA Portal V17? Kind regards |
Follow us on