4/27/2021 10:27 AM | |
Joined: 12/3/2018 Last visit: 3/23/2025 Posts: 12 Rating:
|
Hello everyone, I would like to seek your expertise on dealing with analog input on a CPU 314C-2PN/DP. I tried so many things in searching some solution why I can't read or receive a value on my analog input channel 0 using with my simulator 4-20mA. CPU online simulation: When I use direct address (%IW800), the value is always steady in zero. and when I use peripheral address (%IW800:P), value is always steady in 32767. PLCSIM simulation: Analog value is doing fine when I modified value from 0...27648 I checked from the analog card manual for the wiring connection. I tried to apply all from the manual but the same problem. Maybe there is something I miss? attached is the screenshot during simulation with CPU and PLCSIM simulator. Really appreciated for your help. Thanks in advance. keep safe. AttachmentSimulation Screenshot.zip (485 Downloads) |
4/27/2021 9:10 PM | |
Joined: 12/3/2018 Last visit: 3/23/2025 Posts: 12 Rating:
|
Hi Duris_I, The default address of the cpu 314c-2pn/2dp integrated analog input is 800...8009. I already changed to 752. I checked my simulator output using multi meter and it doings fine from 4...40mA. attached images for your info. thanks. Autogen AttachmentAI overflow to 32767.zip (549 Downloads) |
4/28/2021 12:03 PM | |
Joined: 12/3/2018 Last visit: 3/23/2025 Posts: 12 Rating:
|
Hi Wizard, Please see attached file. Thank you. sorry for the drawing coz using Paint apps. Autogen Attachmentscreenshots.zip (537 Downloads) |
4/28/2021 12:43 PM | |
Joined: 12/3/2018 Last visit: 3/23/2025 Posts: 12 Rating:
|
Yes...pin 3 (AI current) and pin 4 (AI common). BR, AutoGen |
4/28/2021 1:02 PM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, here is your same Topic: Analog input problem |
With best regards... |
|
This contribution was helpful to
1 thankful Users |