5/17/2017 1:42 PM | |
Joined: 4/28/2015 Last visit: 3/27/2025 Posts: 70 Rating:
|
Hello for all. Firstly, sorry for posting question with OMRON device. I need to connect RFID module omron V680S PDF and cpu S7-1511c-1 PN. I did the folowing: 1. Added GSD file to the project 2. Assigned ip, names 3. Downloaded all hardware to CPU Now in TIA portal online view there are not some "red" label with errors, but omron RFID is not working. The led on the body of RFID "LINK/ACT" is flashing continously , in the manual this flashing disribed like "flash during detects carrier" . The led RUN is always green. Perhaps, somebody met this device and worked normaly with it, pls, i hope you can give me advice With best regards,Dmitry. |
Last edited by: hadok at: 5/17/2017 1:43:34 PMLast edited by: hadok at: 5/17/2017 2:03:55 PM |
|
5/17/2017 3:21 PM | |
Joined: 10/1/2013 Last visit: 9/12/2025 Posts: 605 Rating:
|
Hi hadok, how do you know that it's not working? Are you reading and writing the I/O area of the RFID reader in OB 1? |
5/17/2017 4:50 PM | |
Joined: 4/28/2015 Last visit: 3/27/2025 Posts: 70 Rating:
|
Led RUN is always green. If i try to send some bits from wath table (modify 0 to 1) nothing happens. Attachment0-02-05-0956e158d9e8b282b8b65ad5a8e2ef069e8814c73ab7055049dcbaaef1c56e7f_full.jpg (1137 Downloads) |
5/18/2017 8:39 AM | |
Joined: 4/28/2015 Last visit: 3/27/2025 Posts: 70 Rating:
|
Also would like to ask, is this addressing right? |
5/18/2017 1:21 PM | |
Joined: 4/28/2015 Last visit: 3/27/2025 Posts: 70 Rating:
|
Yes, adresses are I 256.0 and Q256.0, so i think i must write in Q258.0 (offset 2) |
Follow us on