10/3/2006 5:07 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Firstly you cannot use V6 SP3 with W2003 SP1 as it is unsupported - stick to V6 SP4. http://support.automation.siemens.com/WW/view/en/21927773 Are you trying to install the AS-OS Engineering during the initial WinCC installation or are you adding it after WinCC has been installed ? -If it's during the initial install, uncheck the box and try to install it seperately. -If you already have WinCC installed can you post the error message here? |
10/3/2006 5:22 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Hmm, very strange.Has anyone else installed these versions: WinCC V6 SP4 Step7 5.4 Windows 2003 SP1 |
10/3/2006 7:50 PM | |
Joined: 5/19/2006 Last visit: 8/21/2025 Posts: 550 Rating:
|
Hi, Can you attach hereMAP_LOG.TXT file from your Windows dir? Dec |
Last edited by: Dec at: 10/3/2006 7:50 PM |
|
10/4/2006 8:48 AM | |
Posts: 16 Rating:
|
Hi, here is the file best regards Lionnel AttachmentMAP_LOG.pdf (515 Downloads) |
10/4/2006 4:40 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
The logreports"ERROR: Setup needsRegedit in Windows directory -> EXIT." !! |
Last edited by: salma at: 10/4/2006 4:50 PMI also note you have a hyphen in your computer name - CLEA-AUTOMATION. This is not allowed with WinCC (see the release notes) and I strongly recommend you uninstall WinCC / SQL Server, change the computer name to remove the hyphen and reinstall. Painful I know but better you know this now at the start and not weeks into a project! |
|