6/18/2018 7:01 PM | |
Joined: 10/14/2017 Last visit: 5/19/2025 Posts: 26 Rating:
|
Hello, I have here a HMI KTP600 Basic that i am programming and i have a problem with the background of certain buttons. First dont know why in this HMI i dont have the function to place the aperance background invisible like i use to do on other basic HMI´s. In result of that i had to place the backgorund of the button matching the rest of the backgrounds; Sometimes in yellow, others grey etc.. But as you can see in the pictures, in some buttons the backgorund does not appear with the propertie that was chosen. So i delete this button, create a new one configure it and perfect... meanwhile a completelty different button in another screen the same thing happens. What am i missing here or is this a really nice bug? PS: plese see photos; AttachmentCapturar.zip (181 Downloads) |
6/18/2018 8:17 PM | |
Joined: 10/14/2017 Last visit: 5/19/2025 Posts: 26 Rating:
|
Yes .png |
6/18/2018 8:41 PM | |
Joined: 4/26/2012 Last visit: 9/16/2025 Posts: 1645 Rating:
|
places an image of the general flap. If you want, send me the project with some of the screens that have the problem and I convert here to do a test. In the time of winccflexible I did it. Murof LINK |
Last edited by: rdoliveira at: 6/18/2018 8:47:33 PMLast edited by: rdoliveira at: 6/18/2018 9:03:30 PM"Always make a backup before performing any tests |
|