10/24/2019 6:54 AM | |
Posts: 7 Rating:
|
Yes, we configure datalog as Siemens described. See attached scrennshots. |
10/24/2019 6:57 AM | |
Posts: 7 Rating:
|
Second screenshot |
10/24/2019 6:59 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
And what does the parameterization of the data log look like? |
10/24/2019 7:29 AM | |
Posts: 7 Rating:
|
On SD card created zero length file 203_0 without any data. |
10/24/2019 8:34 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
@Scorp, to the time, as he make the second pso with the entries, wrote I my post. |
10/24/2019 8:45 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
Not the first 512 entries, that's not right. The buffer for data logging has 1024 Bytes. Is a SD Card in the LOGO!, saved the LOGO! the first 512 Bytes in the buffer before the LOGO! saved the logged datas on the SD Card. See attachment. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 276.pdf (534 Downloads) |
10/24/2019 9:08 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
I did tests. From this it can be seen that the data log is also written if the buffer is not yet filled with 512 bytes. Data Logs are attached. AttachmentData Logs.zip (385 Downloads) |
10/24/2019 10:26 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
Here have news. AttachmentData Logs.zip (291 Downloads) |
10/24/2019 2:57 PM | |
Posts: 7 Rating:
|
Thanka all for replyes. 1. When I trying get DataLog via LSC I receive massage "No datalog found". 2. If I stop Logo and remove SD Card and read them in PC then I found zero length csv file (Program worked 1 week before read SD card) 3. Programm and screenshot of DataLog block properties is attached. AttachmentData Logs.zip (322 Downloads) |
10/24/2019 3:30 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
Hello Nopolis, please be so Kind and upload you program as a ZIP file. Thanks. |
10/24/2019 6:25 PM | |
Posts: 7 Rating:
|
Program in attached zip file
AttachmentVer 9.zip (307 Downloads) |
This contribution was helpful to
1 thankful Users |
10/24/2019 7:19 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
First transferred your uploaded program to my LOGO! 8.FS4. In attachement: AttachmentData Logs.zip (307 Downloads) |
10/24/2019 8:13 PM | |
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
Once again a destroyed program, which can be uploaded to the Logo and don't have all functions. |
10/24/2019 8:23 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
I suggest the User Nopolis to start a Support Request so that Siemens will examined his source program. |
This contribution was helpful to
1 thankful Users |
Follow us on