10/5/2010 11:00 PM | |
Posts: 14 Rating:
|
Hi; Thanks a lot. I had modified the program and S7 STL source file is like this. How can i remove the error generated like Transposition of parameter and missing parameters in FC call in parameter _DB. I am attaching the file. Can anyone help me to remove errors. This is like nightmare!!!!!!!! Chittaranjan sahu
Attachments7 stl.zip (286 Downloads) |
10/6/2010 8:31 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, missing parameters -> i have removed FC257/FC258 from the source file, they are not used You must copy the following blocks from Standard Library\S5-S7 Converting BlocksFC68 FC101 as FC1050
André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools Attachmentnew.zip (276 Downloads) |
10/7/2010 9:32 AM | |
Posts: 14 Rating:
|
Thanks for ur reply. But i do not want to delete FC257 and FC258 as it require in the program. I am introducing FC277[ PB213 in s5] in modification. can any-one help mehelp me to shorted out errors. Thanks in advance!!!!!!
Attachment251004AC_original.AWL.zip (285 Downloads) |
Follow us on