12/5/2022 1:26 PM | |
Joined: 1/5/2012 Last visit: 4/1/2024 Posts: 22 Rating:
|
Ok this time I tried it with TSEND_C and TRCV using the same connection. Again, Data received at Node Red but nothing received at the PLC.
Attachment0.7 TSEND_C and TRCV.zip (864 Downloads) |
12/5/2022 1:58 PM | |
Joined: 1/5/2012 Last visit: 4/1/2024 Posts: 22 Rating:
|
Ok here is another try using 2 ports. 2000 is outgoing port configured as active. 2001 is incoming port. TSEND_C is using connection 1 TRCV_C connection 2. The TRCV_C is setup as a passive connection. CONT := FALSE ADHOC := TRUE listening to port 2001 on connection 2. Again, sending data to node red works fine. I still have yet to receive anything. This is the overall problem. Sending has worked the whole time. Receiving fails. Attachment0.8 2 port TSEND_C and TRCV_C.zip (834 Downloads) |
Follow us on