4/23/2012 2:42 PM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Dear DIVYESH, is the FB250 not available in your CPU or does your CPU not support floating point arithmeticoperations? In second caseyou can purchasean optional package for handling floating point values 6ES5 845-8GP01 "GP115U" (if still available). The package is originaly developed for S5-115U CPU's but will run on95U & 100U as well (just a bit more slower). The other option would be to develop your own blocks. Regards. |
Give us your feedback and show us your respect! |
|
4/23/2012 4:33 PM | |
Posts: 8946 Rating:
|
CPU928A supports floating - point operation, so scaling is absolute no problem! Write a FB by yourself! |
4/24/2012 7:31 AM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Hello BeVee , does this package contains the FB250 he is looking for? I could not find it. Please verify. Regards. Here is the link to the manual of the "Basic Function Blocks" package. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=19394653&caller=view Except the scaling of analog inputs & outputs I could not find any general scaling block. What I still not understand is that when he makes a complete upload to the PG, the FB250 is not getting transferrerd? At least the block header or something should be there or not? Regards. |
Last edited by: TIBI68 at: 4/24/2012 7:52 AMGive us your feedback and show us your respect! |
|
Follow us on