6/4/2013 3:11 PM | |
Posts: 1547 Rating:
|
Hello, first of all you need the GSD file for ET200B, because the ET200B is very old and not in delivery with TIA Portal. The GSD file you will find here: PROFIBUS GSD files : ET 200B Check the correct order numbers. Import GSD file in Device view (Menu Options -> Install G..S…D.. file) to get the ET200B shown in HW list under GSD. Add the Device in Network view and connect with DP Port of S7 300. Set addresses and download. Then you can address the inputs and outputs. Copy the data to DB via Load and transfer code and create HMI variables to access the data in DB. |
6/11/2013 11:07 AM | |
Posts: 30 Rating:
|
Correct me on my attach ladder diagram, Thanks to all Jeff |
6/11/2013 11:14 AM | |
Posts: 30 Rating:
|
Hi Slave126 yeah something like how do i correctly program it. Because i dont have big knowledge of plc programming using the blocks. Thanks and Best Regards Jeff |