4/18/2012 8:28 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello again, But solutions for old posts, they should contain some remarkable points Best regards, Hamid Hosseini |
4/18/2012 9:56 PM |
|
Joined: 4/20/2007 Last visit: 9/1/2025 Posts: 731 Rating:
|
I been wondering what 42 is in binairy code... |
4/19/2012 9:06 AM |
|
Posts: 8946 Rating:
|
fourty-two means "Tea for two" as Douglas Adams explains his universal answer. |
4/19/2012 9:27 AM | |
Joined: 10/3/2010 Last visit: 9/12/2025 Posts: 1568 Rating:
|
Answering old unsolved threads is fine but as soon as an answer is accepted by the mods, imo the thread should be closed (not deleted). |
B r g d s , |
|
4/19/2012 10:01 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello, After the post of Give a star to our expertsNow most of the user are trying to Close the Post by saying Thanks or posting the reply, Let see How much time it will take to adopt all. |
Ammy |
|
4/19/2012 10:28 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
This is my final suggestion our readers to provide feedback if the problem solved by points provided in the thread.The best place would be signature in which most of friends ask for being rated or thanked in case problem clarification.Readers are susceptible to read the signatures or description of users.(as our O_Moderator did it). "So,we can ask readers to provide feedback for solutions" Best regards, Hamid Hosseini |
This contribution was helpful to
3 thankful Users |
4/19/2012 12:47 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
To our S_Moderator- is not be possible that message to be automatically displayed? In some members that kind of message would exceed extra their signature. Best regards, Hristo Mihalev
|
4/19/2012 1:30 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Dear friends, So in the final iteration we reached to a converged solution (conclusion) I try to optimize my signature for sake of community. Let me consult the moderating who can make this suggestion available in public to be widely used, if it is logical. Best regards, Hamid Hosseini |
Follow us on