3/14/2016 10:20 AM | |
Posts: 18 Rating:
|
Hello, I try to Download and upload my program PC --> LOGO!. But he give's an error that says "Transmission error (Timeout. LOGO! does nos respond)" LOGO! 230 RC / PN: 6EDI-1FB00-0BA6 / Com. cable: LOGO! pc cable Isolated (USB CABLE) (COM 8) i try to change the com. port no. but same error come's out... once i click the automatic detection the LSC say../ INTERFACE SELECTION ERROR. Please check: -mode of the logi! : PC<---->LOGO -the LOGO! PC cable connects the LOGO! and the PC. I hope you can help me. Kind regards, Rafhael ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/15/2016 10:43:08 AMNew subject after splitting |
|
3/16/2016 7:00 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
You want to transfer the program from a previous logo in a newer logo? In attachment a video on choosing the right logo type. AttachmentSelect_hardware.wmv (499 Downloads) |
3/16/2016 8:16 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
Can you make a screenshot of the window with the Interfaces? I want see, which COMs you have. |
3/16/2016 8:20 AM | |
Posts: 18 Rating:
|
i can upload it but i cannot download it what is the problem ? :( |
3/16/2016 9:13 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
Which OS do you have? |
3/16/2016 9:15 AM | |
Posts: 18 Rating:
|
windows XP 32bit. I use VMWARE. :) |
3/16/2016 9:28 AM | |
Posts: 18 Rating:
|
i read some article that LSC is worked in windows XP. :3 what OS do you use for your LSC ? maybe the OS must be the problem ? |
3/16/2016 9:56 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
And if you have installed LSC make an upgrade to V8 (via the Update Center). |
3/16/2016 10:08 AM | |
Posts: 18 Rating:
|
how can i move or copy the LSC XP to windows 7 is that possible ? |
3/16/2016 10:12 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
This is to my knowledge not possible. You must install LSC under Win7 new. |
Follow us on