6/23/2022 8:15 PM | |
Joined: 6/22/2022 Last visit: 12/20/2022 Posts: 1 Rating: (0) |
Today 22.06.2022 in our machine we have a isue with fault 50011 - SIMOTION D445. How did this happen? We decided to replace the main transmission of the machine because water got inside it. By default, we turned off the machine, put LOTO on, removed the servomotor - we did not disconnect the cables and replaced the transmission. Then we put everything together, turned on the power and wanted to synchronize the machine. We made it in the standard way, but the machine did not want to calibrate itself. After connecting to the teleservice, he found error 50011 but they don't know how to fix it. It wasn't until the next day that they sent a note to factory reset the D445. We did it twice and after that the machine was synchronized. This procedure factory reset you are founding in manual from Simotion D445. Thanks. PiotrDab ------------------------------------------------------------------------------------------ |
Last edited by: PiotrDab at: 06/23/2022 20:16:24Last edited by: PiotrDab at: 06/23/2022 20:18:46Last edited by: Jen_Moderator at: 06/24/2022 09:38:54New subject after splitting |
|
Follow us on