8/27/2019 1:26 PM | |
Posts: 7 Rating:
|
I try to upload the hardware and software of the PLC S7-1215C with several inverters g120 CU240E-2PN V4.7.6 (project was greate TIA V14.0 SP1). Uploading fails. Message 1 - Could not determine type of module qain GSDML-v2.3-siemens-sinamics-g120-20140313.xml offline. Message 2 - Could not determine type of module EXT GSDML-v2.31-siemens-sinamics-g120-20140704.xml offline. Upload aborted while uploading from device. I found one of the files in the library https://support.industry.siemens.com/cs/ua/en/view/109741558 But I can’t download this library, where can I still get only the two files mentioned above? It’s possible to somehow create or remake them from other GSDML files? |
Last edited by: Jen_Moderator at: 08/27/2019 14:04:11Optimized link. |
|
8/27/2019 3:16 PM | |
Posts: 7 Rating:
|
Free to download Energy Support Library V1.0(for usage with Energy SuiteV14), other version after checking user data. I'll try this library, later unsubscribe. |
7/10/2024 1:31 AM | |
Joined: 5/23/2014 Last visit: 9/9/2024 Posts: 1 Rating:
|
SINAMICS STARTER - ID: 26233208 - Industry Support Siemens this software can solve it |
Last edited by: Wit_Moderator at: 07/10/2024 12:55:00Link optimized |
|
Follow us on