5/10/2007 10:53 PM | |
Posts: 7 Rating: (0) |
Everytime I do a COLD boot of the PC when it restarts I have to go to SIMOTION OPC FILE MANAGER and reimport the xml file to communicate with the Simotion PLC. |
5/22/2007 11:26 AM | |
Posts: 1 Rating: (0) |
Hi, what you are discribing may be possible when using a pc with an embedded operatating system on it. For example, XPembeddedtells you, the fileis be writing on C: ; but C: is a flash ; the the file can't be stored. After a cold start, the file does no longer exist and therefor you have to reimport . Please contact me. I think we will solve this problem. My eMAil: franz-josef.weigert@siemens.com |
Follow us on