4/25/2019 4:53 PM | |
Joined: 11/5/2014 Last visit: 11/5/2024 Posts: 16 Rating: (5) |
Here is attached S7-1200 sample project.AttachmentLKSol_SampleS7-1200_20190425.zip (1175 Downloads) |
8/22/2019 1:30 PM | |
Joined: 11/5/2014 Last visit: 11/5/2024 Posts: 16 Rating: (5) |
If anyone is interested here is video how to set up basic IEC104 connection: Dont forget to enable subtitles as they actually inform whats going on :-) also on lksol.eu there are newer version of library and also "manual" |
Last edited by: Jen_Moderator at: 08/23/2019 09:30:10Embedded Video. Last edited by: LakomyM at: 08/23/2019 18:17:38 |
|
This contribution was helpful to1 thankful Users |
8/23/2019 2:33 PM | |
Joined: 11/5/2014 Last visit: 11/5/2024 Posts: 16 Rating: (5) |
and I've also made up the setting up of the IEC61850 with conversion to IEC60870. (Also dont forget to enable subtitles) |
Last edited by: LakomyM at: 08/23/2019 18:18:34 |
|
3/18/2020 12:02 PM | |
Joined: 11/5/2014 Last visit: 11/5/2024 Posts: 16 Rating: (5) |
If anyone is still interested I have made some changes in the libraries and now you can try any size of datapoins even without valid key. The connection will reset after about 1000 sent or received packets for IEC60870 and about 50 sent packets for IEC61850, so plenty of time to test it :-) |
This contribution was helpful to1 thankful Users |
7/11/2021 7:04 PM | |
Joined: 2/2/2021 Last visit: 5/18/2023 Posts: 3 Rating: (0) |
Hi, anyone is aware where i can downloa dteh last version of IECtest sw ? Thanks |
5/17/2023 7:48 PM | |
Joined: 8/3/2018 Last visit: 5/17/2023 Posts: 1 Rating: (0) |
Please, can update the link
|
6/11/2023 5:31 PM | |
Joined: 1/19/2010 Last visit: 8/4/2024 Posts: 1 Rating: (0) |
Its amazing Can you share the library? The link to download is broken
|
Follow us on