1/3/2023 11:50 PM | |
Joined: 9/27/2006 Last visit: 10/14/2024 Posts: 12287 Rating: (2685) |
Translation from the Spanish text:
Hola Mrtin; El foro de Siemens atrae a participantes del mundo entero, y toos no hablan español. Para facilitar los intercambios en este foro hemos escogido el inglés como idioma internacional. Haznos el favor de escribirnos en inglés a su próxima visita (o usa un traductor electrónico como Google Translate si lo necesita). Hello Mrtin; The Siemens forum attracts participants from many countries, and many do not understand Spanish. To make exchanges easier between us, we have chosen English on the forum as a common language. Please write to us in English on your next visit (or use an electronic translator such as Google Translate, if needed). When you say you need the "register entry of the current value" are you looking fir the current count value of the HSC? This note from the following HSC_CTRL FAQ could provide the informtion you require: https://support.industry.siemens.com/cs/ca/en/view/41995947 Note The current counter value for the "Control high-speed counters" [CTRL_HSC] operation is not provided for in the parameters. The address for the process image is assigned to the high-speed counter in the hardware configuration and includes the current counter value. You can read out the counter value directly via the program logic. The value output in your program is a correct counter value for the moment in which the counter was read. The actual counter value can therefore change before your program has completed a process with an old counter value. Maybe these application examples can provide hints on working with S7-1200 HSCs. https://support.industry.siemens.com/cs/ca/en/view/109742346 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/03/2023 23:51:37Last edited by: dchartier at: 01/04/2023 15:17:44 |
|
This contribution was helpful to1 thankful Users |
Follow us on