11/18/2013 5:51 AM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello Shobuz, Yes it is possible with AOP, and not possible with BOP. Please note that you have to delete at least one language from AOP to use upread feature due to memory limitations. Operating Instructions: ADVANCED OPERATOR PANEL (AOP)
Read page 7: Memory Limitation The delivered AOP supports five European Languages of English, German, French, Spanish and Italian. Due to internal memorylimitations the user should delete one of these languages in order to upread the specified ten parameter sets that can be held on the AOP. To Delete a Language To do this Select “Language” from the top level menu, highlight the language you want to delete then press “Fn” and “↑”. Please notethat once a Language has been removed it cannot be restored. |
Last edited by: Ste39 at: 11/18/2013 6:14 AM |
|
11/18/2013 10:34 AM | |
Posts: 25 Rating: (0) |
hello , gd aft try this link how u can upload / download mm440 |
10/27/2021 4:26 PM | |
Joined: 10/27/2021 Last visit: 10/27/2021 Posts: 1 Rating: (0) |
merhaba SAYFA BULUNAMADI
|
Follow us on