3/24/2023 9:57 PM | |
Joined: 9/22/2021 Last visit: 5/14/2024 Posts: 3 Rating:
|
Can you explain detsil , how you changed the LAN ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/27/2023 11:46:52New subject after splitting |
|
3/27/2023 2:15 PM | |
Joined: 7/19/2022 Last visit: 9/11/2024 Posts: 383 Rating:
|
Hello Usama92, You must go to SIMATIC Shell > Properties and select the network card via which ES-OS communicates. In addition, ES and OS must be visible in SIMATIC Shell, for which you can review these points: What are the requirements for operating SIMATIC WinCC in a Windows network? |
If this Information really helps, you could use the Rate function |
|
3/28/2023 12:49 PM | |
Joined: 8/3/2009 Last visit: 9/11/2024 Posts: 13647 Rating:
|
Hello Usama92 If you are working with WinCC V7/8 or WInCC Professional then check this FAQ: https://support.industry.siemens.com/cs/de/en/view/108464289 Its one of the basic FAQs which you need almost at every WinCC station to set up correcly. Here you will also find how to set up the simatic Shell Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on