8/14/2023 12:44 PM | |
Joined: 8/7/2023 Last visit: 5/11/2024 Posts: 3 Rating: (0) |
Hello everyone, I'm new to SIMATC STEP7 environment, I've created a small project with S7-400 hardware interface with profibus slave device, it doesn't show any error while compiling but showing error message when downloaded into hardware. Diagnostic buffer message can be found in the attachment it shows I/O access error when updating the process image input table P area, double-word access, access address: 0 process image partition no.: 0 not user relevant(Z1): 2942 Requested OB: Program execution error OB (OB85) OB not found, or disabled, or cannot be started in the in the current operating mode External error, Incoming event. Can anyone help me with this issue? Thank in advance AttachmentDiagnose_msg.txt (538 Downloads) |
Last edited by: Jen_Moderator at: 08/15/2023 04:06:00Shortened headline. |
|
8/15/2023 4:15 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject I/O access error when updating the process image input table P area, double-word access, access address is published within the conferenceSIMATIC S7-400 / S7-400H / S7-400F /FH. Best regards, |
Follow us on