1/26/2024 9:48 AM | |
Joined: 7/19/2022 Last visit: 8/6/2024 Posts: 380 Rating:
|
Hello Ziemens, The way I do it is the following: 1. Create a button to export recipe data to a USB or SD card. 2. You load the project but without checking the option to overwrite the RT values. 3. In the RT you save the .csv from the created button. 4. You upload that .csv to the engineering project and you would already have the RT recipes in engineering. Therefore, you can now make modifications having all the data. |
Last edited by: JBS98 at: 01/26/2024 09:49:09If this Information really helps, you could use the Rate function |
|
Follow us on