6/26/2024 1:38 PM | |
Joined: 10/21/2022 Last visit: 8/21/2024 Posts: 4 Rating: (0) |
Hello. PCS7 9.1V. The same issue but with one difference. On ES we have few users and now if ADMIN user logged in then OS disappeared from project in simatic manager. With other user OS visible on project tree. I try to delate mdf and ldf files. but no any success. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/27/2024 06:07:13New subject after splitting |
|
6/26/2024 6:22 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
Hi, It looks related to the user. I would look into the user rights. Make sure SIMATIC HMI rights are active at least. Pleas check Compendium part A for more info. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
6/27/2024 5:55 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
That's good to hear! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on