8/10/2024 7:47 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, In the following link you can find the released modules for PCS7. Please select the correct version before opening the document. Siemens is using the CPU410-5H as the only controller used for PCS7. This CPU can handle everything like standard operation or redundant setup, with/without safety functions. Before the CPU410-5H there were a lot of CPU's like CPU414, 416, 417, 417 redundant and so on. With the CPU410-5H they rely on only one controller. It's the best CPU, but you can scale it according to your needs in the form of AS PO. If your application become larger, you won't need to replace the CPU for a bigger one. You already have it with the 410. The only thing is that you increase the amount of AS PO in the CPU. The "H" in the name means high availabilty and does not mean it's a CPU with redundant capability only. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on