2/29/2016 7:21 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Hi DaytonaM, I think this is a problem with the SQL database. For this, open SQL Enterprise Manager and find the database under WinCC/Databases which has a grey color instead of orange. It means that the database is corrupt or locked or is in "suspect" mode (also indicated at the end of the database name). I also had this problem once, after VersionDoc program makes a copy of the WinCC database, but it cannot delete it's own database after it's done. Simatic Manager will react to this by removing the OS station, sort of protection mode. After deleting the database, restart Simatic Manager and check to see if the OS station is back. |
Last edited by: Oreca at: 2/29/2016 7:23:18 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/10/2018 8:32 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
Hi, No problem! This is a weird problem indeed...but as I mentioned earlier, it looks like some sort of protecting mechanism to prevent corruption of your OS project, or it is just a bug. But glad it solved your problem. I know people who didn't know the solution earlier and they reinstalled the whole ES |
If I could help you, you can use the RATE button. Thank you. |
|
4/11/2018 8:08 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
Hi Tekabi, see below:
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on