1/22/2021 4:08 PM | |
Joined: 7/2/2015 Last visit: 6/21/2024 Posts: 96 Rating: (23) |
Dear Priyanka B, To do a backup of the panel I recomend you to read the FAQ How do you backup/restore with a Comfort Panel? |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
1/26/2021 8:03 PM | |
Posts: 3 Rating: (0) |
It is fine with HMI but what about automatic backup with SIMATIC S7-1500 PLC? How can I access the memory location of backup file which is stored in internal memory of PLC ? Is it possible to give the path of the backup file from program of PLC to take automatic backup from PLC? Please answer. Thanks, Priyanka B |
Follow us on