8/21/2024 4:44 AM | |
Joined: 5/27/2024 Last visit: 9/14/2024 Posts: 8 Rating: (0) |
What is the difference between 6ES7653-2BA00-0XB5 - SIMATIC PCS 7, software, Runtime License AS(PO 100) and 6ES7658-5AX68-OYA5. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/21/2024 06:28:13New subject after splitting |
|
8/21/2024 5:24 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
Hi, The license: 6ES7658-5AX68-0YA5 is the AS/OS engineering and you need this to work with Simatic Manager to do engineering work and WinCC work. The Runtime license AS RT PO is a quantity license and should exist on the engineering station. During download of CFC charts, the system determines the amount of process objects. A process object could be a valve or motor. Then the amount of required PO is booked from the engineering to the CPU.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on