7/2/2024 8:55 AM | |
Joined: 6/19/2024 Last visit: 7/2/2024 Posts: 3 Rating: (0) |
Hello, After many hours of research, I cannot find the reason for my problem, and I haven't found anything conclusive in the existing topics... I have a Siemens S7 1500 that I am trying to communicate with an HMI based on Windows 10 on a Galium screen. I specify that I am using a switch. For a reason I deeply don't understand, I can download screens to it, but I cannot connect to it! It is unreachable. However, I can see it on the TIA Portal, I can ping it, the IP addresses are correct... I have already tried connecting it directly to the CPU, changing the IP addresses, disabling ALL Windows protections on the HMI, etc., but it still doesn't work. What is strange is that I cannot see it when I try to connect using the "same IP address" criterion, but when I choose "compatible device" I can see it and the IP address is indeed the same... And once again, I can download screens to it, so they must be communicating, BUT I cannot establish a link. Do you have any suggestions? I should mention that I am a beginner; the forum has already helped me a lot. Thank you in advance for your time. Here is my configuration: AttachmentHMI.pdf (128 Downloads) |
7/2/2024 9:05 AM | |
Joined: 5/18/2022 Last visit: 9/4/2024 Posts: 56 Rating: (1) |
Hi!! Do you have created the HMI connection? Ex: |
If this Information really helps, please let me know by rating me :) |
|
7/2/2024 9:10 AM | |
Joined: 4/24/2006 Last visit: 9/26/2024 Posts: 8742 Rating: (1168) |
Hello, Perhaps this link might help: Best regards, Wizard |
This contribution was helpful to1 thankful Users |
7/2/2024 9:22 AM | |
Joined: 6/19/2024 Last visit: 7/2/2024 Posts: 3 Rating: (0) |
I'll take a look, thanks! |
Follow us on