10.09.2024 10:33 | |||||||||||||||||||||||||||||||
Beigetreten: 18.12.2014 Letzter Bes: 02.10.2024 Beiträge: 33866 Bewertung: (4210) |
SSA-103653: Denial-of-Service-Sicherheitslücke im Automation License Manager
SUMMARY In der Automation License Manager-Software wurde eine Sicherheitslücke festgestellt, die durch das Senden speziell gestalteter Pakete an Port 4410/tcp eines betroffenen Systems ausgelöst werden könnte. Dies könnte zu einem Denial-of-Service-Angriff führen, der legitime Benutzer daran hindert, das System zu verwenden. Siemens hat eine neue Version für Automation License Manager V6.2 veröffentlicht und empfiehlt, auf die neueste Version zu aktualisieren. Siemens empfiehlt spezifische Gegenmaßnahmen für Produkte, für die Fixes nicht oder noch nicht verfügbar sind. AFFECTED PRODUCTS AND SOLUTIONUn-/Collapse All
WORKAROUNDSANDMITIGATIONS Siemens has identified the following specific workarounds and mitigations that customers can apply to reduce the risk:
Product-specific remediations or mitigations can be found in the sectionAffected Products and Solution. GENERAL SECURITY RECOMMENDATIONS As a general security measure, Siemens strongly recommends to protect network access to devices with appropriate mechanisms. In order to operate the devices in a protected IT environment, Siemens recommends to configure the environment according to Siemens' operational guidelines for Industrial Security (Download:https://www.siemens.com/cert/operational-guidelines-industrial-security), and to follow the recommendations in the product manuals. Additional information on Industrial Security by Siemens can be found at:https://www.siemens.com/industrialsecurity PRODUCT DESCRIPTION VULNERABILITY DESCRIPTIONUn-/Collapse All This chapter describes all vulnerabilities (CVE-IDs) addressed in this security advisory. Wherever applicable, it also documents the product-specific impact of the individual vulnerabilities. Vulnerability CVE-2024-44087 Affected applications do not properly validate certain fields in incoming network packets on port 4410/tcp. This could allow an unauthenticated remote attacker to cause an integer overflow and crash of the application. This denial of service condition could prevent legitimate users from using subsequent products that rely on the affected application for license verification.
ADDITIONAL INFORMATIONFor further inquiries on security vulnerabilities in Siemens products and solutions, please contact the Siemens ProductCERT:https://www.siemens.com/cert/advisories HISTORY DATA
TERMS OF USE Siemens Security Advisories are subject to the terms and conditions contained in Siemens’ underlying license terms or other applicable agreements previously agreed to with Siemens (hereinafter "License Terms"). To the extent applicable to information, software or documentation made available in or through a Siemens Security Advisory, the Terms of Use of Siemens’ Global Website (https://www.siemens.com/ terms_of_use, hereinafter "Terms of Use"), in particular Sections 8-10 of the Terms of Use, shall apply additionally. In case of conflicts, the License Terms shall prevail over the Terms of Use. SSA-103653 ©Siemens 2024 |
||||||||||||||||||||||||||||||
Für diesen Beitrag bedanken sich1 Benutzer |
Folgen Sie uns auf