2/16/2024 9:26 AM | |
Joined: 2/15/2024 Last visit: 2/25/2024 Posts: 24 Rating: (0) |
Hi, I was also waiting for the MQTT integration. After some trial and error I was able to update my LOGOSoft Comfort version 8 to 8.4 on my old Macbook Pro. But now I have 3 older modules installed since several years: - 0BA7.ES4 with firmware version V1.03.37 As you can see, these are modules from V7 (many years ago). I don't think I can just update the firmware to make them work with 8.4 ? I believe I will need to buy 3 new blocks instead. But if that's the case, I do have another question about my "extension modules". For each module above, I have added an extension module with serial number 6ED1055-1NB10-0BA0: https://mall.industry.siemens.com/mall/en/ww/Catalog/Product/6ED1055-1NB10-0BA0 This module is off course also discontinued, but would it work with a new 8.4 module? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/16/2024 10:43:29New subject after splitting |
|
2/16/2024 10:17 AM | |
Joined: 2/15/2024 Last visit: 2/25/2024 Posts: 24 Rating: (0) |
Ok, thank you for your reply. Thanks again. |
2/16/2024 1:08 PM | |
Joined: 12/18/2014 Last visit: 10/19/2024 Posts: 33999 Rating: (4228)
|
The 6GK7177-1MA20-0AA0is the successor. |
2/16/2024 1:13 PM | |
Joined: 2/15/2024 Last visit: 2/25/2024 Posts: 24 Rating: (0) |
Thanks ! |
This contribution was helpful to1 thankful Users |
Follow us on