5/9/2024 1:11 PM | |
Joined: 7/4/2012 Last visit: 9/12/2024 Posts: 2 Rating: (0) |
I am trying to establish communication between an ET200SP CPU 1512-1PN with CM DP Module (6ES7 545-5DA00-0AB0) and an S7-316-2DP. I have downloaded the file from the corresponding link for the ET200S CPU + CM DP module which I integrated into step 7 of my S7-300. Unfortunately, it is not working. Error message with the GSD into STEP7 for hardware of S7-300: The type of plugged-in module differs from the configured one. Thank you for your help ! ------------------------------------------------------------------------------------------ |
Last edited by: allyouneed at: 05/09/2024 14:51:06Last edited by: Jen_Moderator at: 05/10/2024 07:41:38New subject after splitting. Text formatting optimized. |
|
5/10/2024 7:42 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subjectHow to establish communication between a CM DP Module and an S7-316-2DP. is published within the conference Communication / Networks. Jen_Moderator |
Follow us on