(0)| 2/24/2011 1:42 PM | |
|
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, have you allready try a direct connection without a switch? best regards. |
| 2/24/2011 4:30 PM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Dear KGP, It's possible to reset panel to factory settings You will have to perform an OS update with the option "Reset to factory settings" See the following link: how do you do an operating system update (OS update) on operator panels? Also have a look at this link: how do you integrate an HMI operator panel into a local network? You have to change the "device name" of the panel. Best regards, Wizard |
| 5/11/2011 12:52 PM | |
|
Joined: 5/28/2008 Last visit: 1/15/2026 Posts: 1344 Rating:
|
Have you made an HMI connection between Panel and PLC? |
| 5/11/2011 1:13 PM | |
|
Posts: 2 Rating:
|
Yes I did. I set to obtain IP automaticly and static IP on panel, this didn´t work as wel. |
| 7/30/2025 4:49 AM | |
|
Joined: 4/18/2024 Last visit: 12/6/2025 Posts: 1 Rating:
|
Is your problem solved..? |
Follow us on