2/10/2018 9:26 AM | |
Posts: 2 Rating: (0) |
Hi All experts, I am trying to develop a Energy monitoring project for my home. I have designed my system with PAC3200 & PAC1200 device. Designed model is in attachment. My designed equipments as follows. PAC3200 Energy meter 2 Nos 7KT PAC1200 Data Manager 2 Nos S7 1200 CPU 1212C 1 Nos 7KT 3 Sensor Bar 8 Nos 7KT 40A Sensor 24 Nos I wanted to monitor through web & android apps all the circuit breakers data. Can anyone give me any demo programe of a such kind of designed & physical connection diagram. Is there anything else do i need? please help. Thanks & best regards Khyru AttachmentEM Diagram-Model.pdf (467 Downloads) |
2/13/2018 7:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
Hello, Exact FAQ as per your requirement is not available, however please refer below FAQ which may help you. powermanager Quick StartData Communication between S7-1200 and SENTRON PAC3200 via MODBUS TCP (Set 22) |
Last edited by: Jen_Moderator at: 2/13/2018 1:24:36 PMOptimized links. |
|
Follow us on