(0)| 12/17/2006 2:02 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="Ravi"]Is there something that can be done using Kepware driver. I already have that and I do not want to get the CPs and REDCONNECT in this. We have a whole lot of customized applicationbuilt on .Net platform that we have tested using Kepware driver. Hi Ravi, Because I use with the MP370WinCC Flexible to switch to another internal link, I think it is not that easy to switch with Kepware. Thisis solved in WinCC Flexible with switching the connections over an TAG. So one of the CPUs have the connection. Put a MP370 on a H-System with Ethernet With REDCONNECT you have always contact with both CPUs, there is a redundant connection between the CPs and the CP1613. Normally I recommend REDCONNECT, so that customers have something where I could say that it works for 100%. I never tried, but have heared from other people that it is easy to make a connection to a H-System wenn everything is ok, but when there are some errors in the communication then it is not that easy to couple to the right CPU. With REDCONNECT you have a 100% balanced product whats testedfor several years (2000...2006) in a lot of goodworking systems, it also have a OPC-Server, so I don't understand the problem. A customer that have a H-System don't want not-tested configurations in his system, therefor he want to pay something more if that is giving him a garanty that it works. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on