11/25/2013 9:03 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, It seems you have PLC-SIM installed. It's to simulate a PLC for testing your programs. There is a manual here: S7-PLCSIM Regards, Marcjan |
Problem solved? |
|
11/27/2013 12:23 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Please find the basic procedure in attached document. It's not mutch different from a real PLC, you need to download the hardware and blocks like if it's a real one. regards, Marcjan Attachmentplc_sim.pdf (906 Downloads) |
Problem solved? |
|
12/2/2013 8:17 AM | |
Joined: 9/2/2012 Last visit: 6/3/2019 Posts: 176 Rating:
|
HelloSAMIRKM. To my knowledge. all you have to do is open plcsim from simatic (press on the menu "Options") and then click the row that says "Simulate modules" and then press "Select CPU access node" from the file-menu in plcsim. When plcsim is running, the PC/PG interface is automaticly set to plcsim and needs not to be changed manually. When you have selected the CPU access node, select the connection you have on the intended cpu, like mpi or profibus and press ok, then its just to set the cpu mode to "Run-P" and upload your code normally.
|
9/20/2021 7:14 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by wishy is split to a separate thread with the subject Download a program with PLCSIM. Best regards |
Follow us on