5/8/2018 5:38 PM | |
Posts: 3 Rating:
|
Thank you Daniel, I contacted Siemens support and will post my findings on this thread. |
10/2/2018 10:27 AM | |
Joined: 1/16/2017 Last visit: 7/25/2025 Posts: 2 Rating:
|
Hi All, I had this exact fault using TIA portal V14 SP1 Had a 1515-2PN CPU and a CM1542-5 Profibus module in the rack 8 x ABB FPBA-1 Profibus slaves on the network. ABB nodes kept dropping off when i went online in TIA Portal direct at Slot X1. Got in touch with ABB and they suggested changing the GSD file from ABB10959.gsd to a ABB0959.gsd It fixed the problem. Something to do with DPV0 and DPV1. # Attached the GSD files sent to me by ABB AttachmentFPBA-01_GSD_files (3).zip (832 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on