9/17/2025 2:51 PM | |
Joined: 4/28/2015 Last visit: 9/18/2025 Posts: 3 Rating:
|
Hello, Working with the LPallPatt library ID: 109800960, Downloading the example LPallPatt_V3_3_0_GettingStarted_TiaPrj_V19 and simulating with S7-PLCSIM Advanced V6.0 in TIA Portal V19.0.3, trying to load two different pallets generated in the editor with interlayers enabled i.e. height over 0 mm after each other does not update productPositions array in DB LPallPatt_Data correctly. Data that is there is from the first loaded pallet with interlayers, correct positions are however displayed in the HMI under Edit Layers. Somehow loading a pallet generated in the editor without interlayers, height to 0 mm, always seems to work correct in that productPositions array in DB LPallPatt_Data is correct. It's possible to get pallet generated with interlayers to load correctly into PLC if load of pallet without interlayers are loaded in-between/before. Thanks for the help, |
Follow us on