10/5/2012 2:25 PM | |
Posts: 14 Rating:
|
Hello, I wanted to try SIZER for Siemens Drives software so I downloaded latest version v3.7 and tried to install it on real computer with "used" Win7_Pro_x64 and virtual machine with "clear" WinXP_Pro_x32_SP3. Installation was not successfull because.. 1. problem was with MS SQL server 2008 - SQL server installation failed (SIZERSetupLog file with "Exit Code: -289740454") I had only one idea how to solve it - download different SQL Server 2008 Express installer from. http://www.microsoft.com/en-us/download/details.aspx?id=1695 One by one I renamed SQL installers to SQLEXPR.exe (name of the original installer distributed within SIZERv37.zip), replaced original one and tried to run "main" SIZER setup.exe. I tried all releases: SQLEXPR_x86_ENU.exe - worked for Win7x64 (WinXPx32 not tested) SQLEXPR_x64_ENU.exe - didn't work SQLEXPR32_x86_ENU.exe - worked for WinXPx32 (didn't work for Win7x64) 2. problem came when SIZER installation had to start (after Start button press). Error meassage immediately popped up saying: "Sizer for Siemens Drived setup signaled errors. (Operation finished successfully). See log files:" ..\\SIZERSetupLogg_xxx_.txt and ..\\SIZERMSISetupLog_xxx.txt SIZERSetupLog.txt is attached (ending with Exit Code: 2). MSILog was not created at all.. Same result with Win7 and WinXP. From this point I didn't make any progress. I can't find any explanatory notes for Exit Codes. BUT I managed to install SIZER_v3.6 on virtual machine with WinXPx32. After replacing SQL installer with renamed SQLEXPR32_x86_ENU.exe whole installation process was without a problem and SIZER is able to run. Can anyone give me any advise about v3.7 installation? thx Matus
AttachmentSIZERSetupLog_2012-10-05_132934.zip (679 Downloads) |
Follow us on