7/23/2021 12:42 AM | |
Joined: 9/1/2020 Last visit: 3/24/2024 Posts: 12 Rating:
|
mmm i have just uninstalled TIA portal V16 because of i had many errors i dont have pic of the errors but also i can not visualize in the step7 v5.5 in the simatic manager the HMI's as if the project were not integrated i had to uninstall and the problem continues, i am uninstalling manually from the register the communicationsettings program. and now i am reinstalling step 7 in order to see if now is possible visualize the HMI, because of there were problems with the PC station. defined in the original step7 project ------------------------------------------------------------------------------------------ |
Last edited by: Eduardo_2020 at: 07/23/2021 00:42:51Last edited by: Eduardo_2020 at: 07/23/2021 00:43:56Last edited by: Jen_Moderator at: 07/23/2021 09:48:26New subject after splitting |
|
Follow us on