8/15/2025 2:12 AM | |
Joined: 6/21/2025 Last visit: 8/15/2025 Posts: 1 Rating:
|
怎么根据MAG6000序列号查询变送器的生产批号 |
Last edited by: Moderator_Lan at: 08/15/2025 07:49:38Title translated |
|
8/19/2025 10:48 PM | |
Joined: 3/28/2010 Last visit: 9/12/2025 Posts: 1172 Rating:
|
The Modbus RTU manual is attached. The Modbus RTU slave register map shows the "batch cycle counter" as Holding Register (4)02252 (one-based addressing) or 2249 (decimal zero based addressing) on page 47 (pdf) of the 2010 Modbus RTU module manual (attached). That value is a 4 byte Dword. Since the manual describes some values as 4 byte values as "floats" (presumably IEEE754 floating point), a Dword is most like a 4 byte, 32 bit integer. Modbus devices are not addressed by their serial numbers, Modbus devices are assigned a slave node ID number (1-247). But, the converter's serial number is available via Modbus. Register(4)02521 has the converter serial number as a 20 byte string, presumably ASCII characters (page 54, pdf) AttachmentUSMII_MODBUS_AOM_OI_En_en-US.pdf (191 Downloads) |
Follow us on