3/23/2010 5:40 PM | |
Joined: 8/31/2005 Last visit: 9/12/2025 Posts: 2198 Rating:
|
Hello raghu, - The FM458 is not a typical SIMATIC module, main use is close loop control, it must be programmed with CFC and D7-SYS (versions of software must match) After you understood the different philosophy (to SIMATIC S7), it is simple. - See the getting startedandthis document (It describes the T400, a small stand alone module similar to the FM, but has more backround informations; read up to chapter to 6.8.2) -The normal way is to use the standard blocks (there are about 300 types). Sometimes it may be unconfortable, but 99% of the users where able to program the required function. If required, you can buy D7-SYS-Gen and program your own blocks in C (look the older threads in this conference). What do you want to do with the FM458? |
Last edited by: miami at: 3/29/2010 10:25 AM |
|
3/25/2010 7:39 AM | |
Posts: 3 Rating:
|
thanks Dirk We are using the FM 458 for Automatic gap control for Cold rolling mills . |
Follow us on