5/16/2011 12:50 PM | |
Posts: 2964 Rating: (482)
|
Hello.... Does your motor having a brake if it is not released also you have this error too.... you can also disconnect the motor outside from the mechnicals and run it in JOG mode if it moves smoothly then you need to check your mechnical parts again...... Are checked the Power module IGBTS diodes with help of multimeter it could be also module problem too.... Check this attachment refer pg no: 3 /tf/WW/en/Posts/45570#top Regards, Ekalavya |
10/16/2023 9:03 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Hello Rejjal, thank you for your efforts! Regarding repairs, I have received a recommendation from the Product Management:
Best regards, |
This contribution was helpful to1 thankful Users |
Follow us on