10/23/2024 9:21 AM | |
Joined: 5/12/2023 Last visit: 1/8/2025 Posts: 3 Rating:
|
Hello bg2492, I am a little late for the discussion but i am currently working in a project where i need to implement a similar functionality. I want to make the text list dynamic, where a VB script gets data from a txt file and insert certain values (text strings) and output it to the operator. Do you know a way (VB functions ...) to update the text list with the VBS that is triggered with a button. Thanks. PS : I have WinCC V7.5 and PCS7 V9.1 SP2 with CEMAT V6.1 ------------------------------------------------------------------------------------------ |
Last edited by: badr_ramdani at: 10/23/2024 09:22:09Last edited by: badr_ramdani at: 10/23/2024 09:24:39Last edited by: Moderator_Lan at: 10/23/2024 09:27:58New subject after splitting Regards, |
|
10/23/2024 9:52 AM | |
Joined: 7/11/2024 Last visit: 8/4/2025 Posts: 200 Rating:
|
Hello Have you tried with a Combo Box through script? Check the following: How can the combo box configured in the OS be filled dynamically with texts of different languages? Hope it works! |
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on