10/29/2024 4:54 PM | |
Joined: 1/2/2024 Last visit: 1/6/2025 Posts: 23 Rating:
|
Hello, I hope you are very I want to ask a question I have the same IOT but the pre-installed indOS did not work either, I managed to connect via UART and changed the boot mode, which started with the SD but then how do I install the operating system on the system and make it work without the SD, what would be the steps to follow? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/30/2024 08:53:24New subject after splitting |
|
Follow us on