11/18/2024 10:50 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Yogendr_Tiwari, In this case, to perform the migration you want I recommend you to review the following FAQ that I share with you: In the "Download" section you have a PDF that indicates the process to migrate from V6.2 to V8. There you will find the steps until you reach V7.5 which is the version you need. I also recommend you to always update until the last update of the version to make the jump to the next version. I encourage you to review this documentation to see if it can help you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on