6/24/2025 9:19 AM | |
Joined: 12/1/2006 Last visit: 7/18/2025 Posts: 25 Rating:
|
Hello, I appreciate very much the I/O field option “Operator message” : if you set it to yes, it creates a usefull purple message in the Operation List that states who, when, previous and new values setted in the tag connected to the output value. I would like to do the same for a button that toggle ON /OFF a variable . When an operator click the button the script simply check the variable and if it is 1 set it to 0 or viceversa. I would like that in the message list appears a string like : “ Variable Name, Username , Old value = 1 New value =0 ”. I tired to follow the eample here ( I have WinCC 8.0) : https://support.industry.siemens.com/cs/de/en/view/24325381 But it doesn't work. First the string is not the same type of alarm of I/O Filed. And also there is nothing written. In the operation list appears a gray empty line. Have you got any idea?
|
Last edited by: Moderator_Lan at: 06/24/2025 10:26:31link optimized |
|
Follow us on