(0)| 8/27/2025 11:14 AM | |
|
Joined: 6/4/2015 Last visit: 8/29/2025 Posts: 3 Rating:
|
840D sl, after a restart, the 7 segments is flashing 3-3-4-6. and all leds lits orange. What happens or changes when you remove the FAN/BATT module or even when the CF-CARD is not inserted? If nothing changes with the status leds and the generated code on its display, than properly the BOOT section/sector is defect (firmware). Communication with the NCU is not possible in any way, also the USB port will not work either and you can better replace the NCU buy a new one. If someone else has found an explanation or another solution instead of replacing the module, please let me know. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/27/2025 11:20:09New subject after splitting Last edited by: unis-jw at: 08/28/2025 10:53:33 |
|
Follow us on